Two or more cameras can share a bus, but you must manage packetsize. Divide the packetsize by the number of cameras per bus to avoid
HALER_NOBUSRESOURCES returned on OpenCapture().
FGP_CARD tracks the number of buses per controller. In this sense “Card” means “bus”, NOT physical card count (some cards have multiple bus controllers).
CFGCamera Camera[NMAXCNT];
UINT32 NodeCntPerCard[NMAXCNT],Card[NMAXCNT];
```// Step through node list
for(i=0;i<NodeCnt;i++)
{
// Connect device to object
Camera[i].Connect(&NodeInfo[i].Guid, &Camera[i]);
// Get number of cameras per card
Camera[i].GetParameter(FGP_CARD, Card[i]);
NodeCntPerCard[Card[i]]++;
}
...
// Set format, divide payload
UINT32 Speed(0),PktSize(0);
for(i=0;i<NodeCnt;i++)
{
// Set Format 7, Mode 0, Y8
Result=Camera[i].SetParameter(FGP_IMAGEFORMAT,MAKEIMAGEFORMAT(RES_SCALABLE,CM_Y8,0));
// Get phy speed
if(Result==FCE_NOERROR)
Result=Camera[i].GetParameter(FGP_PHYSPEED, &Speed);
// Divide PacketSize by number of cameras
if(Result==FCE_NOERROR)
PktSize=(1024<<Speed)/NodeCntPerCard[Card[i]]);
// Set PacketSize
if(Result==FCE_NOERROR)
Result=Camera[i].SetParameter(FGP_PACKETSIZE, PktSize);
if(Result==FCE_ADJUSTED)
Result=Camera[i].GetParameter(FGP_PACKETSIZE, &PktSize);
// Start DMA logic
if(Result==FCE_NOERROR)
Result=Camera[i].OpenCapture();
}