Topics related to Allied Vision’s GigE Vision cameras.
Are there some details about the interpolation algorithm of the Manta G-201 camera RAW2RGB picture?
Hi leeyang,
Manta G-201c camera uses a 2 × 2 matrix for Bayer demosaicing.
Please refer to the chapter Color interpolation (Bayer demosaicing) of our Manta User Guide:
There is a question I want to confirm. After the interpolation, (Bayer demosaicing on Page 267 of the Manta_TechMan.pdf) will one pixel be lost in both horizontal and vertical directions?
At the border a respective color pixel value from the nearest neighbor is used to get the most reasonable value. The last pixel is not lost. Resolution remains the same comparing BayerRG8 and RGB8Packed pixel formats for instance.