Topics related to Allied Vision’s FireWire cameras (IEEE 1394)
Dies ist eine Antwort zu Topics related to Allied Vision’s FireWire cameras (IEEE 1394)
When using Vimba SDK to retrieve camera timestamp by accessing ulong AVT.VmbAPINET.Frame.Timestamp, it is desirable to be able to convert it to real time in seconds instead of camera ticks. However, the available resources only show how to do this by using camera tick frequency in Ethernet AVT cameras, but not in FireWire cameras. What would be the correct alternative to that in FireWire models?
The timestamp of FireWire cameras is given in Nanoseconds as well. TickFrequency=1GHz.